Download document () of 20

BladeUPS frequently asked questions

The Eaton BladeUPS is a three-phase, modular UPS for high-density computing environments. This UPS can provide back-up power for 5 kW in 6U of space all the way up to 60 kW (N+1) in a single rack enclosure by deploying additional modules in an easily scalable, building-block fashion.

Is the Eaton BladeUPS a three-phase UPS system?

Yes, Eaton BladeUPS is a three-phase input and output UPS system, with base designs at 208V for the North American market and 400V for international markets. 

Where is the BladeUPS system manufactured?

The BladeUPS is manufactured in North Carolina, USA. 

What is the kVA and kW rating of each BladeUPS module?

Each module is rated for 12kVA and/or 12kW. It’s important to note that the kW rating is more important than kVA for this specific product due to the very high power factor (typically 0.95–0.99) of the computing equipment that BladeUPS is designed to support. 

How much rack space does one BladeUPS occupy?

Each BladeUPS module takes up 6U of rack space based on the EIA industry standard. Each additional extended battery module (EBM) is 3U. Each “U” is equal to 1.75 inches, so each module is 10.5 inches tall.  

Is BladeUPS available for international voltages and frequencies?

Yes, the BladeUPS is offered at 400V line-to-line or 230V line-to-neutral. This version is also compatible for countries with voltages ranging from 380 to 415 VAC. The BladeUPS provides auto-frequency sensing. The unit adapts to and runs at the input frequency it senses at start-up. 

Is the BladeUPS system delivered fully configured?

The BladeUPS system is one of the easiest systems on the market to install, configure and deploy. All systems go through full system testing before they are delivered, so customers can rest assured that components will work together, right out of the box. Even the future expansion of paralleling modules will only require a very simple installation and then a “plug-and-power” procedure. Therefore, while Eaton will offer on-site configuration services, we won’t offer fully configured systems from the factory. 

Is the BladeUPS delivered with batteries installed?

To ensure the cabinet isn’t damaged by the excess weight of the batteries, BladeUPS modules are delivered with the batteries removed. This will also be beneficial for installation as the batteries will not need to be removed from the UPS chassis prior to mounting the system in the IT rack or enclosure. The electronics module and battery packs include a “blind” or self-aligning connector at the rear of each pack to make them very easy to install or remove. 

What type of UPS topology does BladeUPS offer?

BladeUPS offers “hybrid” power technology. This innovative design considers the design capabilities of the actual computer power supplies in such a manner that the UPS furthers that capability, thereby providing a very robust and effective power protection solution. 

What is the efficiency of the BladeUPS system?

During normal operation, the system provides a minimum efficiency of 97%. 

How does the BladeUPS system obtain a high level of efficiency during normal operation?

The BladeUPS adapts to the incoming power source and provides the uninterrupted power the load requires while dynamically selecting the most effective mode of operation. So BladeUPS protects critical loads from poor power quality. 

Can a BladeUPS be paired with a generator?

BladeUPS is a very good option when you need to pair a generator with a UPS. We designed in frequency acceptance windows that help keep the system operating from the generator, even if the generator isn’t as stable as it should be. This ensures that your equipment keeps operating from the generator rather than running the batteries down. 

Does the BladeUPS system work well with data centre or IT applications?

Absolutely. With its exceptional efficiency and flexibility, the BladeUPS was designed specifically for data centre and IT applications, from a single rack to an enterprise data centre. 

Does the BladeUPS protect against transients from the power company?

Yes. The BladeUPS was designed with input filtering capability that meets several engineering specifications to protect IT equipment from lightning or other transients typically seen on AC input. 

If I have noise on the utility input, will that be seen on the output of the BladeUPS?

No. Noise on the input is filtered out through the input design of the system. 

Will the BladeUPS system still provide protection if the generator frequency becomes erratic?

The BladeUPS system was designed to adapt intelligently to changing conditions such as this. In fact, BladeUPS is smart enough to run unsynchronised with the varying input frequencies, therefore giving the output a stable 60 or 50Hz output frequency. It does this without resorting to battery back-up, saving battery capacity for re-transfer when utility voltage returns. 

Do I need an external maintenance bypass for the BladeUPS?

No. Every BladeUPS base chassis includes an automated maintenance bypassing mechanism.

  • In a single BladeUPS system, the mechanical maintenance bypass automatically actuates if hot-swappable electronics or battery modules are removed. This feature ensures that power to protected loads is not accidentally interrupted by human error. 
  • In a multi-module parallel configuration, the system first determines if it is operating in redundancy or capacity mode. 
    • If BladeUPS modules have been paralleled for redundancy, removing an electronics or battery module will not force a transfer to maintenance mode. Only the UPS unit being serviced goes offline, and its load is automatically transferred to other units in the configuration. 
    • If BladeUPS modules have been paralleled for capacity, and maintenance activities could potentially cause an overload condition on other modules, removing a module or taking a unit offline would trigger an automatic transfer to maintenance bypass.