Download document () of 20
  • Power Distribution Monitor and Control banner

    Power Xpert Protection Manager (PXPM)

    Companion software to simplify configuration, troubleshooting and testing of Eaton Power Defense circuit breakers. PXPM is free to download with premium upgrades available.
    How to buy


How to buy PXPM

laptop software icon

PXPM software essentials 

  • Setpoint configuration
  • Real-time data for troubleshooting
  • Event summaries for trips and alarms
  • Coordination of multiple trip curves
  • Breaker open/close testing
  • PDF reports with customisable covers

FREE

testing breaker icon

Advanced breaker testing

1-year licence

  • Includes the essentials
  • Secondary injection testing
  • Current sensor continuity test
  • Pick-up testing
  • Test library
  • Pass/fail results on time-current curve

$289

Breaker testing icon plus

Complete suite

1-year licence

  • Includes the essentials
  • Includes advanced breaker testing
  • Breaker trip/alarm waveform data access
  • Guided troubleshooting wizard
  • Breaker help knowledge base

$312

Looking for earlier versions of PXPM?

You can find legacy licensing available by clicking on the button below.

Core features

Breaker control

  • Capture single-cycle waveforms, open the breaker or reset the trip unit from PXPM.

     

Change rated current without a rating plug

  • PXPM allows changes to any rated current (in) supported by the breaker frame on Magnum and Power Defense insulated case circuit breakers.  Unlike traditional rating plugs, which require changing the breaker’s CTs and use a different plug for each rating, PXPM provides a quick, fully digital solution.

Setpoint configuration with time-current curve visualisation

  • PXPM provides an intuitive interface to configure your breaker setpoints.  Visualise changes on the time-current curve as you adjust.  Import setpoints from multiple breakers to coordinate curves or duplicate settings between units. 
  • Make changes while connected to the breaker, or at your desk to share with colleagues or load to devices later.
A powerful test suite lets the user easily verify their current sensors, breaker trip functionality, and any point on their time-current trip curve.  Interactive guidance ensures that the breaker is correctly configured for testing to ensure accurate results.​

Customisable reports

  • Create printable PDF reports of real-time data, breaker settings and setpoint changes, captured waveforms and results of performed secondary injection tests, customisable with customer information.
Exportable PDF reports, with customizable cover, make it easy to test results, setpoint changes (as-found vs as-left), and events on the breaker.​

Troubleshooting tools at your fingertips

  • PXPM supports breaker troubleshooting with real-time data and historical information such as trip and alarm event details, waveforms and breaker runtime conditions. 
  • Guided troubleshooting and tips are available to jump-start your troubleshooting efforts. 

Advanced testing suite

  • Traditional secondary injection testing involves bulky test kits and only verifies part of a breaker’s functionality.  PXPM’s advanced testing can verify ampacity along the trip curve with nothing but a standard USB cable.  This unique offering also validates every part of the breaker without the cost, wear and time requirements of primary injection testing conducted by a third party.
  • PXPM makes testing easy to perform, without requiring special skills or equipment.  Tests can be set up in seconds. Pass/fail criteria interpret the results and present them in tabular form or on a trip curve.  Test reports are available to download as PDF or CSV.  
A powerful test suite lets the user easily verify their current sensors, breaker trip functionality, and any point on their time-current trip curve.  Interactive guidance ensures that the breaker is correctly configured for testing to ensure accurate results.​
Pass/Fail results summary and log of tests along the trip curve makes testing easier than ever.

   Circuit breaker testing FAQ

What is primary injection testing? 

In primary injection testing, large currents are injected into the primary side of the breaker, exercising the sensors and protection circuitry.  This allows complete testing of all parts of the circuit breaker, but it is time consuming and costly.  This also has an impact the length of the breaker’s life, as it creates stresses on the device. 

What is secondary injection testing?

For a secondary injection test, current is injected in parallel with the output of the current sensor, representing the output of that sensor. All the built-in protection circuitry and routines respond as per the settings in the breaker. 

This test does not assess the functionality of the current sensor. 

What is current sensor continuity testing? 

The current sensor test verifies continuity and functionality of breaker’s current sensors. 

PXPM performs this test by proprietary circuitry in the PXR trip unit to generate a signal that is directed through the Rogowski coil.

What is complete functional circuit breaker testing?

PXPM combines secondary injection testing with sensor continuity testing to test all parts of a circuit breaker. 

The complete testing of the breaker may be an acceptable alternative to a primary injection test of the breaker. 

What is simulated functional testing?

This is when the firmware is given the simulated current value to test itself at. 

PXPM performs this test by using issuing a command to the trip unit with the value of current the tester has requested.   This assessment is primarily performed as a second-level test when troubleshooting. 

What is curve testing? 

Curve testing verifies various points on the time-current curve, and operation of the breaker based on different situations. This can be used to verify that the trip unit’s protection algorithms are functioning properly. 

PXPM performs this by varying the signal during secondary injection testing. 

PXPM can also achieve this through the simulated functional test. 

What is pass/fail testing? 

Pass/fail testing is a convention of reporting the outcome of each test instead of just data. 

PXPM is programmed with the breakers’ time-current curves to automatically summarise the results of the testing.  PXPM reports a time for LSIG and determines the outcome of the test based on the time-current curve. 

How are test reports used?

Test reports summarise the details of the testing performed.  Frequently, these are manually created based on results from the testing equipment. 

PXPM provides a detailed summary of the testing performed in PDF format.  This report can be customised with details of the breaker’s name or location. 

X
Download Close