For more than ten years, DIN EN 60204-1 has ensured the safe design of electrical equipment for machines and plants. The underlying IEC 60204-1 standard was updated in 2016 - now the European version of the world's most widely used machine safety standard is published. This whitepaper provides an overview of the most important changes for machine and plant manufacturers, especially with regards to switchgear technology.