HDMI explained
HDMI means High-Definition Multimedia Interface, a standard for simultaneously transmitting digital video and audio from a source, such as a computer or TV cable box, to a computer monitor, TV or projector. Originally developed by a consortium of electronics manufacturers, it has been widely adopted with almost all televisions and computer monitors supporting the interface.
The goal of the HDMI initiative back in 2002 was to improve on existing connectivity standards (e.g. DVI, component video) by creating a smaller connector, adding support for embedded audio and delivering a higher resolution video signal. Such was HDMI's success that by 2008, shipments of HDMI-enabled devices exceeded those of DVI. By the end of 2009, all HDTVs had at least one HDMI port.
HDMI connectors are available in three sizes: standard, mini and micro.
There are also different types of HDMI cable (see the chart below). Not all cables use the logo but the cable specifications should indicate whether it is standard, high speed, Premium High Speed or Ultra High Speed. If the type is not indicated, assume standard.
| CABLE TYPE | RESOLUTION | BANDWITH |
|---|---|---|
| Standard (category 1) | 1080i or 720p | 4.95 Gb/s |
| Standard with ethernet | 1080i or 720p, plus a dedicated HDMI ethernet channel | 4.95 Gb/s |
| High speed (category 2) | 1080p or 4K @ 30 Hz | 10.2 Gb/s |
| High speed with ethernet | 1080p or 4K @ 30 Hz, plus a dedicated HDMI ethernet channel | 10.2 Gb/s |
| Category 3 (4K) | 4K @ 60 Hz | 18 Gb/s |
| Category 3 (8K) | 8K @ 60 Hz or 4K @ 120 Hz | 48 Gb/s |
HDMI cables are available in male and female versions, with space-saving right-angled connectors and gripping or locking connectors. HDMI cables are considered low voltage so you can install it inside a wall. HDMI faceplates give a clean, finished appearance and have a female connector on the internal side, making termination easy. HDMI keystones are also available for digital signage applications and large conference facilities with many displays that are fed from a central location.
The majority of HDMI connectors in use today are the Type A (standard), Type C (mini) and Type D (micro) shown below. HDMI Type B (dual link) was developed for very high-resolution displays but was never used. Also not shown is the HDMI Type E connector which is intended for automotive and industrial applications.
Gripping and locking HDMI connectors
HDMI connectors do not latch like DisplayPort connectors but some do provide a spring mechanism that makes the blade of a male connector grip the receptacle and makes it less likely that the cable will be accidentally pulled out. If an HDMI device may be subject to vibration or accidental movement, use a connector with a screw lock.
Which is best, in-wall HDMI cable or wireless HDMI?
A cable connection is a relatively inexpensive option that gives a strong, reliable signal but can be difficult to install, it's limited to one location and a distance of 25-50-ft., depending on the resolution. Longer distances require an active cable or HDMI extender. A wireless HDMI extender is much easier to install, can be easily relocated and can broadcast a high-resolution video signal to multiple receivers.
Note: In-wall HDMI cables have a CL2 or CL3 rating. This means that the cable jacket is fire resistant and suitable to low-voltage in-wall applications.
Is there a difference in functionality between the standard, mini and micro HDMI connectors?
All three connectors have the same 19 pins, but some may have different pin assignments. Functionally, they all support the resolutions and features of HDMI 1.4 onwards.
Can a USB-C port be used to transmit HDMI to a monitor?
Yes. In Alt Mode, some of the pins in a USB-C connector are used to transmit other protocols. This allows the widely adopted USB-C port/connector to be used for more than just USB data or power. To date, there are four Alternate Modes: DisplayPort, Mobile High-Definition Link (MHL), Thunderbolt and HDMI. HDMI Alt-Mode supports all of the features of HDMI 1.4b, including video resolutions of 4K @ 30 Hz and above.
I need an HDMI cable for my 4K TV, what should I buy?
Buy a high speed HDMI cable that supports at least HDMI 1.4, the first HDMI standard to support 4K signals. To get a 4K picture, all components must support 4K: the cable box or streaming service, the HDMI cable and the TV. If you are using an old standard HDMI cable purchased before 2009, it will not have the bandwidth to carry a 4K HDR signal.
| SPECIFICATION | YEAR | VIDEO | AUDIO SUPPORT | ||
| Max resolution refresh rate* | Max transmission rate** | HDR | |||
| HDMI 1.0 | 2002 | 1080p @ 60 Hz | 4.95 Gb/s | No | 8 audio channels |
| HDMI 1.1/1.2 | 2005 | 1440p @ 30 Hz | 4.95 Gb/s | No | DVD-Audio, One-Bit Audio |
| HDMI 1.4 | 2009 | 4K @ 30 Hz | 10.2 Gb/s | No | ARC, Dolby TrueHD, DTS-HD |
| HDMI 2.0 | 2013 | 4K @ 60 Hz | 18.0 Gb/s | Yes | HE-AAC, DRA, 32 audio channels |
| HDMI 2.1 | 2017 | 8K @ 60 Hz | 48.0 Gb/s | Yes | eARC |
HDMI 1.0
HDMI 1.4/1.4a
HDMI 1.1/1.2
HDMI 2.0
HDMI 1.3/1.3a
HDMI 2.1
Transition-Minimized Differential Signaling (TMDS) – When digital data is transmitted, especially over long distances, it is susceptible to noise and signal loss. TMDS is a way of encoding an HDMI signal to protect it from interference as it travels from source to receiver. It works like this:
Consumer Electronic Control (CEC) – This feature allows a user to control up to 15 connected HDMI devices using one remote controller. Most TVs and streaming devices support CEC but it may be turned off by default. Manufacturers sometimes refer to CEC using their own branded term (e.g. Anynet+, Viera Link) so it may not be apparent that your device supports it.
High-Bandwidth Digital Content Protection (HDCP) – this authentication protocol allows a sending and receiving device to verify each other's credentials (stored on each device's Extended Display Identification Data (EDID) chip) and, if every checks out, create a shared key that is used to encode and decode the data passing between them. This process, known as a handshake, happens almost instantaneously at the beginning of a session and ensures that an unauthorized device cannot intercept the data as it travels between two devices. In the United States, HDCP support is mandated by the Federal Communications Commission (FCC).
Display Data Channel (DDC) – The HDMI interface includes support for VESA DDC, a set of protocols that allow a source (a computer's graphics card, for example) to ask a monitor what audio and video formats it can handle, and adjust settings on the monitor, such as brightness and contrast. The information exchanged by a source device and a display is called Extended Display Information Data (EDID) and is transmitted through the Display Data Channel.
Chroma subsampling – Chroma subsampling is a form of video data compression. It reduces the amount of color data in a video signal in such a way that there is little or no visible impact on image quality.
Each pixel in a video image includes information on brightness (luma) and color (chroma). Since human eyes are more sensitive to differences in brightness than color, chroma subsampling reduces the amount of data transmitted by allowing pixels to share color data with adjacent pixels.
Chroma subsampling is represented as three digits. The first number is the number of pixels in each row of the sample. The second number indicates the number of pixels in the TOP row that have color information. The third number indicates the number of pixels in the BOTTOM row that have color information.
Color spaces and Deep Color – A color space is a defined range of colors that can be represented in an image. The two primary color spaces used to represent digital video are RGB and YCbCr. Two important characteristics of a color space are Color Depth and Gamut. Color Depth is the number of bits used to represent the color of a single pixel and determines the amount of shading or gradation. Gamut refers to the number of colors available.
The initial HDMI specification provided support for 24-bit Color Depth (8-bits per color x 3 colors RGB). HDMI 1.3 introduced Deep Color, which added support for 30-bit, 36-bit and 48-bit color depths. It's worth keeping in mind that the human eye can only distinguish around 10 million different color, so 24-bit color is adequate for most situations.
| COLOR DEPTH | BITS PER COLOR | ALSO KNOWN AS | GAMUT | HDMI SPECIFICATION |
| 24-Bit Color | 8 | True Color | 16.7 million | 1.0 |
| 30-Bit Color | 10 | Deep Color | 1.073 billion | 1.3 |
| 36-Bit Color | 12 | 68.71 colors | ||
| 48-Bit Color | 16 | 281.5 trillion |
Audio Return Channel (ARC) – Most TVs connect to a sound bar or AV receiver using an optical cable. ARC enables a TV to send audio back to a sound bar or AV receiver through the same cable that delivered the HDMI signal to the TV. In other words, video and audio to the TV and audio back to the sound bar (the "return" part). The benefits of ARC include fewer cables, use of the TV remote to control sound, and the ability to transmit higher resolution audio, such as Dolby TrueHD or DTS HD Master Audio, to your sound bar or receiver. [Version 1.4]
HDMI Ethernet Channel (HEC) –First introduced in the HDMI 1.4b specification, HEC allows Ethernet-enabled devices to share an Internet connection. It combines the features of an Ethernet cable into the HDMI cable, thereby avoiding the need for a separate Ethernet cable. Xbox 360 and Roku are two examples of devices that can take advantage of HEC to connect to the Internet. [Version 1.4]
Dynamic HDR – High Dynamic Range (HDR) is achieved by sending additional information with the video signal that tells the TV or monitor how to display the content. It results in greater brightness, contrast, and better color accuracy as compared to Standard Dynamic Range (SDR). Dynamic HDR simply means the dynamic range can be set on a per-scene basis (or frame-by-frame in the case of high-end TVs).
Enhanced Audio Return Channel (eARC) was introduced in HDMI 2.1 and provides support for higher-quality audio bandwidth and speed. eARC requires a High Speed HDMI cable with Ethernet or an Ultra High Speed HDMI cable. eARC is not backwards compatible with ARC but some products may support both eARC and ARC. [Version 2.1]
Display Stream Compression (DSC) – HDMI is uncompressed audio and video. The higher the resolution, color depth and frame rate, the more bits need to be transmitted until the maximum bandwidth is reached. Then, the only way to transmit more bits is to add more lanes to the cable or compress the signal.
HDMI 2.1 introduced support for Display Stream Compression (DSC) 1.2a, a visually lossless compression for ultra-high definition (UHD) video. Using DSC, an HDMI 2.1 cable can support a maximum compressed bandwidth of 128 Gbps (sufficient for 10K, although it will be some time before there are commercially available devices that need that much bandwidth).
A passive HDMI cable is a simple cable assembly with an HDMI connector at each end. Passive cables have a limited range (more on this later). Active cables on the other hand include a signal booster that enables video and audio to be transmitted over longer distances. Active cables sometimes require a power supply.
Passive cables – Opinions vary over the maximum length of a passive HDMI cable. Consensus seems to be about 50 feet for 1080p and 25-feet for 4K video, but distances of over 50-feet are achievable. A good practical approach is to try a passive cable and, if you have problems with signal strength, add an in-line signal booster at the receiver end. Eaton Model Number B122-000-4K6 will boost a 4K/60 Hz signal up to 50-ft and B122-000-60 will extend a 1080p/60 Hz signal up to 125-ft.
Active cables – Length is more definitive in the case of an active cable because signal transmission is designed and tested over the advertised distance. For example, Eaton's P568-065-ACT active HDMI cable will support video transmission up to 65-ft.
When transmission distance requirements exceed the limits of passive and active cables, it's time to consider the various forms of signal extension.
In-Line HDMI signal extender – For distances up to 50-feet, an in-line equalizer or repeater can extend a 4K/60 Hz signal up to 50 feet and a 1080p/60 Hz signal up to 125-ft. Greater distances are possible at lower frame rates.
HDMI over Cat5 and Cat6 – A Cat5/6 extender will convert the HDMI signal into similar Ethernet IP packets that can be transmitted over the category cable and reconverted at the other end with no loss of signal strength or fidelity. Using this approach, an HDMI signal can be transmitted about three times further than an active HDMI cable–approximately 100 meters (328 ft.). Shielded (STP) Cat6 cable is recommended for its ability to reduce EMI interference from power lines and crosstalk within the cable.
HDMI over fiber – The connectors on fiber HDMI convert conventional electrical inputs to pulses of light that are transmitted at high speed through optical fiber, then converted back to electricity on the receiving end. Since signal transmission is optical, it isn't subject to EMI/RFI line noise. HDMI over Fiber can be extended well beyond the 100 meter/328-foot limit of copper Ethernet cable.
Wireless HDMI extenders – A hardwired extender uses an Ethernet or Active Optical Cable to pass data between a transmitter and receiver. A wireless extender sends the HDMI signal using one of the WiFi protocols (e.g. 802.11ac or 802.11n). Wireless is generally slower than hardwire so make sure the video resolution and frequency is sufficient for your needs. For example, Eaton's B127-1A1-WHD1 can extend a 4K/30 Hz signal up to 98-ft.
Can I connect a TB3 port to an HDMI display?
Yes, but not directly. Thunderbolt 3 has native support for DisplayPort and from DP you can get to HDMI by way of an adapter. You can also use an adapter cable like Eaton's U444-006-H4K6BE to convert DP Alt Mode to HDMI.
Can I connect DisplayPort to an HDMI display?
Yes, a DisplayPort to HDMI adapter cable allows you to connect a computer with DisplayPort video output to an HDMI-enabled monitor or TV. If you use a passive cable, make sure the video source is a DP++ (DisplayPort ++) dual-mode port. If your graphics card does not support DP++, use an active cable such as Eaton P582-006-HD-V2A.
Can I connect a DisplayPort monitor to an HDMI port?
Yes. Even though HDMI and DisplayPort use different signal protocols (TMDS vs. LVDS), it is possible to convert HDMI to DisplayPort with no loss of image quality using an active adapter. The adapter may require an external power source. The Eaton P130-06N-DP-V2 4K HDMI to DisplayPort Active Adapter uses power from the USB-A port.
Can I connect an HDMI port to a DVI monitor?
Yes, HDMI and DVI video signals are compatible. An HDMI to DVI adapter will support resolutions up to 1920 x 1200. However, DVI will not support HDMI audio.
USB Alt Mode allows a USB-C connector or port to transmit non-USB signals, making it extremely versatile. For example, a laptop, Chromebook or Android phone might use Alt Mode to directly connect a USB-C port to an HDMI-enabled monitor without the need for an adapter. This is an important feature because many laptops and tablets have a USB-C port but no HDMI port.
To take advantage of HDMI Alt Mode, you need a USB-C port that supports USB Power Delivery. It is the PD handshake that establishes an Alt Mode connection. You will also need a cable with a USB-C connector on one end and a USB-C or HDMI connector on the other. Older USB-A cables do not support Alt Mode.
Another option is to use an adapter cable supporting DisplayPort Alternate Mode, such as Eaton's U444-006-HDR4BE, to connect a USB-C port to an HDMI display.
As a general rule, video and audio can be converted from one protocol to another equal or lesser protocol as the table below shows. Protocol conversion requires an adapter.
| TO | ||||||
| HDMI | DisplayPort | DVI | VGA | USB-C | ||
| FROM | HDMI | Yes* | Yes** | Yes** | Yes** | |
| DisplayPort | Yes** | Yes* | Yes** | Yes** | ||
| DVI | Yes* | Yes** | ||||
| VGA | Yes** | Yes* | ||||
| USB-C | Yes** | Yes** | Yes** | Yes** | Yes* | |
Switches and splitters are often confused and for good reason. They perform similar functions. A switch takes multiple inputs and lets you choose which one to display on your TV or computer monitor. A splitter does exactly the opposite. It takes a single video signal and replicates it to multiple displays.
HDMI splitters
An HDMI splitter takes one HDMI video signal and sends it to multiple displays. Each display will show the same image. Splitters are often classified according to their inputs and outputs. For example, a 2-port splitter might be referred to as "1x2" because it has one input and two outputs.
When choosing a splitter, make sure the output is at the resolution and frequency you want. A video splitter may also perform protocol conversion, for example, converting DisplayPort to HDMI.
HDMI Switches
An HDMI switch, also called a presentation switcher, outputs audio and video from multiple sources but only one at a time. For example, a boardroom presentation might include Powerpoint slides and video from a streaming service like YouTube or Vimeo.
A matrix switch has multiple inputs AND outputs. For example, a 9x2 matrix switch has 9 inputs and 2 outputs.
Another variation on the many-to-one theme is the multiviewer, which consolidates a number of video inputs on a single monitor. Multiviewers are found in broadcast control rooms and video surveillance systems.
Can I extend my desktop using an HDMI splitter?
No, an HDMI splitter takes one video signal and replicates it to multiple displays so each display shows the same image. This is known as "mirroring". Here are your options for extending your desktop:
A power surge is typically a brief increase in voltage due to, for example, an overloaded circuit, power outage or lightning strike. A surge protector detects excess voltage and safely diverts it through the building's grounding system so it doesn't damage connected equipment.
HDMI surge protectors are intended to supplement primary surge protection and are installed "in line" between a video source and display.
Important: surge protectors do not provide two-way protection against power spikes. If you want to protect both source and display, you should install two surge protectors: one with its output facing the video source and one with output facing the display.
Do in-line surge protectors degrade the HDMI signal?
All in-line surge protectors introduce a small impedance into the line and a capacitance across the line. Eaton's in-line HDMI surge protector (Model Number B110-SP-HDMI) is designed with lower line capacitance and impedance to avoid Transition Minimized Differential Signaling (TMDS) loss.
An HDMI signal includes both video and audio, which is convenient because you need only one cable to connect a cable box, game console or streaming device to your television. But if you want to play audio through an older analog sound system that doesn't have HDMI support, you will need to separate the audio track from the video. That's where an audio extractor comes in.
An HDMI audio extractor splits an HDMI signal into a separate HDMI signal and an audio output. Depending on the capabilities of the audio extractor, you may have the choice of compressed or uncompressed (LPCM) audio outputs, for example, 3.5mm stereo or a multi-channel format like 7.1 surround sound via TOSLINK.
When buying an audio extractor, make sure the video and audio output formats match the capabilities of your television and sound system.
HDMI and DisplayPort are similar standards with a different focus. HDMI has been widely adopted by consumer electronics manufacturers. DisplayPort's main focus is computer connectivity and professional audio/video applications.
If you need to connect a Blu-Ray player, cable box, game console or streaming device to your television, HDMI is the logical choice. Your options for connecting a computer monitor to your laptop or desktop PC may be less clear. Many computers (and docking stations) offer both HDMI and DisplayPort. Which one will give you the best results? In terms of image quality, there isn't much difference. DisplayPort 2.1 has a higher bandwidth, allowing it to support higher resolution video, but there are currently few applications requiring video beyond 4K. However, if you need multiple displays, you can daisy-chain three 4K monitors @ 90 Hz or two 8K displays @ 120 Hz.
| HDMI 2.1 | DISPLAYPORT 2.1 | |
| RELEASED | 2017 | 2019 |
| TYPICAL APPLICATION | Consumer TVs | Computer monitors |
| MAX TRANSMISSION RATE | 48 Gbps | 77 Gbps |
| MAX RESOLUTION (UNCOMPRESSED) | 4K @ 144 Hz 5K @ 60 HZ 8K @ 30 HZ 8K @ 120 HZ (DSC*) |
4K @ 240 Hz 8K @ 120 Hz 16K @ 60 Hz |
Is DisplayPort better than HDMI?
It depends on the specific use case and individual requirements.
HDMI is a widely adopted and widely used standard for connecting audio-video devices, such as TVs, computer monitors, and Blu-ray players. HDMI supports high-definition video and audio, and is supported by most consumer electronics manufacturers.
DisplayPort, on the other hand, is a newer interface standard developed for computer and professional applications. It can support higher resolutions, refresh rates, and bandwidth compared to HDMI, and is commonly used in professional and industrial applications.
So, if you are looking for a standard for home entertainment and consumer electronics, HDMI is a good choice. But if you require a higher performance interface for professional or industrial applications, DisplayPort might be the better choice.
With 8K TVs and cameras now readily available, first adopters are turning their attention to even higher resolutions, including 10K and 16K, and refresh rates above 60 Hz.
Bandwidth is the biggest barrier to higher resolutions and refresh rates. Ignoring all of the extra data layered on top of the video itself, the simple formula (resolution x refresh rate x color depth) adds up to a lot of bits which need to be moved from a video source to a display. An uncompressed 8K, 24-bit color video signal at 60 Hz needs almost 50 Gbps of data bandwidth.
The current HDMI specification tops out at 8K/120 Hz so a revision will be required to go beyond that.